Browse FAQs



How to navigate through an Network Air FM unit display
... Network Air FM unit display. Only qualified service personnel should make ... ... MultiCool® ( chilled water) and ... ... point in the room . ... , then the cooling setpoint is used ... If the room temperature is 23 ... ... point of the room is 26° ... ... between the actual room dew point and the desired room dew ... to control the room environment or if ... ... work as a single System. ... Half capacity uses one compressor and half ... Rooms with small heat ... avoid over- cooling while dehumidifying. When the unit is in dehumidification ... ... the modes ( cooling , reheat, ...
Batteries discharged to a low voltage in a single phase Symmetra frame
1 .) If a battery module ... chargers are commanded off in order to cool the battery and prevent the situation from getting worse.
How to read a pressure temperature chart for super-heat and sub-cooling calculations
... and sub- cooling calculations. All DX Cooling units . Single -component refrigerants ... and condense at one temperature for a ... ... Therefore, only one column is needed ... (see Figure 1 ) ... , more of one component will transfer ... ... of temperature from one side of the ... ... defined by a single pressure-temperature ... Imagine a room full of vapor ... ... each temperature: one for the saturated ... ... only separated by 1 or 2 psi ... ... will only list one column for these ... ... higher glide ( greater than 5° ... ... as for a single -component refrigerant ...
DAC, Cancoil Installation Manual
Section 1 . Warranty and ... Section 1 . ... designed to provide years of reliable performance ... stable, efficient year round operation for ... ... provided in the unit . DO ... SECTION OF THE UNIT . Unit Placement and Mounting ... unit should be securely ... structural base to prevent movement. ... clearance around the unit for proper servicing and preventative maintenance ... ... are based on 1 degree per 100 ... ... be sized to prevent excessive pressure drop ... ... a rate of 1 ” drop per ... ... vertical risers to prevent liquid and oil ... ... be sized to prevent excessive pressure drop ... ... a rate of 1 ” drop per ...
Refrigerant charging table for a Uniflair Unit
... for a Uniflair Unit . ... -cooled DX units must be connected ... ... refrigerant lines/ chilled water piping are ... ... vertical riser to prevent oil from returning ... 1 . Open any shut-off valves present in the system to ensure that all of the components will be tested. ... 1 . Open any shut-off valves present in the system to ensure that all of the components will be evacuated. ... 2. Connect a vacuum pump to the service ports on the system piping. ... Install a ball valve before the micron gauge to prevent damage to the micron gauge during charging.
Where can I get support for APC and MGE Products?
Assessment Services ... Battery Replacement Services ... Data Center Facility Cooling - Andover Continuum or TAC Vista ... Environmental Monitoring Unit ... Fluid Coolers ... High-Density Cooling Enclosures ... InfraStruxure for Server Rooms ... InRow Chilled Water ... Installation Services ... MGE Service Bypass ... Network Integration Services ... On Site Service ... Planning Tools and Publications Portable Cooling ... Power Distribution Units ... Project Management Services ... Remote Monitoring Services ... Room Cooling Accessories ... Row Cooling Accessories ... Service Bypass Panel Service Plans ... Start-Up Service Stationary Power Distribution Units ... Training Services ... Uniflair Chilled Water
Guidelines for installation of an acsc100, or acsc101
Room preparation ... . Ensure the room is insulated to ... room must be sealed ... The room should be thoroughly ... room should have a ... ... airflow for each unit supported. ... of heat per unit . Receiving the unit ... Your InRow SC unit has been factory tested and inspected prior to shipment. To ensure that you have received the unit in excellent condition, perform a careful inspection of the crating and the unit immediately upon receipt. ... If necessary, contact the APC technical service department at 1 -888-695-6500 for help in repairing or replacing damaged parts.
Why do I need refrigerant traps in my piping?
... All Air Cooled Cooling Units Data Center Cooling ... the riser by one pipe size to ... Figure 1 shows the proper ... ... This approach will prevent oil from being ... figure 1 ... always install a single trap at the ... A: Schneider Electric does not require a discharge line muffler nor do we recommend one . ... Warranty issues will be based upon Platform Engineering and, or the District Service Manager discretion. ... A: Whenever a condenser is located above the compressor, an inverted trap or check valve should be installed at the condenser inlet to prevent liquid refrigerant from flowing backwards into the compressor during off cycles.
What are the operational conditions for an InRoom (Stulz) Unit
... (Stulz) Unit . The InRoom precision air conditioning units operate within the following ranges: Room Conditions: ... Frequency:60 Hz +/- 1 % Chilled water-/ cooling water pipes: ... Maximum equivalent length of piping between the cooling unit and the air cooled condenser: 60 m (200 ft) Maximum level difference between the condenser and the cooling unit : 5 m (16 ft) when the condenser is below the cooling unit ... Cooling fluid (DX): 30% Glycol ... Chilled water medium (CW): 0% Glycol
What is the difference between an InRow RP, InRow RD (600mm), and InRow RC (600mm)?
Data Center Cooling ... These units are the equivalent to an InRow RP with the exception that they do not have the equipment for electric reheat and humidification control. If you purchase one of these it is required to have the proper load. The minimum required kW for 1 direct expansion unit is 12kw and 12kw for chilled water. ... Due to the lack of heaters in the RD and RC, there is no dehumidification of the room over the normal cooling of the space.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.