Browse FAQs

Why does the PowerChute service not automatically restart following an upgrade to OpenJDK 16 ?

Published date: 05 January 2021

Issue:
The PowerChute service does not automatically restart following an upgrade to OpenJDK 16.

Product Line:
PowerChute Business Edition v10.0.2

Environment:
SUSE Linux Enterprise Server 15 SP2

Solution:
Follow the below steps to resolve the issue:
1. Open the PBEAgent file located in the /usr/bin directory.
2. Search for “jdk-16(2)” in line 75. Refer to the below screenshot as an example.
3. Remove “(2)”. For example, update this line to read: 'JAVA_RUNTIME=/opt/APC/PowerChuteBusinessEdition/Agent/../jdk-16/jre/bin/java'
4. Navigate to the PowerChuteBusinessEdition directory and delete the empty “jdk-16” folder. Modify the name of the “jdk-16(2)” directory to “jdk-16”.
5. Manually restart the PowerChute service. To restart enter /etc/init.d/PBEAgent restart.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.