Browse FAQs

Galaxy VX; How to set up, stop or change the “Automatic Battery Test” option of the UPS

Published date: 21 January 2020

Issue:
How to set up, stop or change the “Automatic Battery Test” option of the UPS



Product line:
Galaxy VX - all


Environment:
All


Cause:
How to set up, stop or adjust the Automatic battery test option


Resolution:
From the home screen on the display select Configuration > Battery > Test.



Set your preferred settings for the automatic battery test:

Battery Test Interval: Select your preferred interval for battery tests.
Choose between: Never, Every 52 Weeks, Every 26 Weeks, Every 12
Weeks, Every 8 Weeks, Every 4 weeks, Every 2 Weeks, or Once a Week.

NOTE: If you run battery tests too frequently it can reduce the lifetime of the batteries.

Battery Test Start Time: Select the time of the day in 24 hour format that
the test should take place and complete with Enter.

Battery Test Day of the Week: Select the day of the week that the test
should take place and complete with Enter.

When all settings have been completed, tap OK to confirm your settings.





 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.