Browse FAQs

What is the maximum cable bundle diameter allowed by the the AR8621 Toolless Hook & Loop Cable Manager, and how long are they?

Published date: 01 August 2019

Issue:
This information is needed to determine what size cable bundles can attach to each AR8621. 

Product Line:
NetShelter Cable Management

Environment:
AR8621

Cause:
The maximum cable bundle o.d. is not noted in the technical specs. 

Resolution:

The 18" hook & loop cable ties included in the AR8621 support a maximum cable bundle of diameter of 6 inch. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.