Browse FAQs

PowerChute Business Edition cannot be installed on 32-bit systems

Published date: 16 July 2019

Issue:
PowerChute Business Edition v10.0 and higher (v10.0+) cannot be installed on 32-bit systems.

Product Line:
PowerChute Business Edition 

Environment:
All supported OS

Cause:
PowerChute v10.0 is bundled with JDK 11, which does not support 32-bit systems.

Solution:
If you require PowerChute on a 32-bit system, install PowerChute Business Edition v9.5, which is the last version to support 32-bit systems. To download PowerChute v9.5, visit the PowerChute Business Edition Product Page.

PowerChute v9.5 will continue to be supported 12 months after the release of v10.0, i.e. January 2020. For more information, see Knowledge Base article FA159606.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.