Browse FAQs

What are the shipping dimensions of the Galaxy 5000 UPS

Published date: 05 June 2019

Issue:
Galaxy 5000 shipping dimensions

Product line:
Galaxy 5000


Environment:
All Product models, all serial numbers


Cause:
Door height clearance


Resolution:
Aids customer in knowing if the UPS on a pallet or its own height on casters will clear the doors when moving to install location.
 
  • Shipping Dims:
    • UPS: 1 @ 37.8X38.58X79.92" H + 1 @ 33x30x76" H + 1 @ 16x14x7" H (2,902.26 lbs, 2 spots due to dimensions)
    • Batt. Cab: 1 @ 40x40x75" H  (2,835 lbs, 2 spots due to dimensions)



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.