Browse FAQs

Do the NetShelter SX 12U and 18U cabinets have the standard SX roof, or are they different?

Published date: 30 May 2019

Issue:
A customer may want to use ladder or troughs atop these cabinets and needs to know if the roofs are different. 

Product Line:
NetShelter SX 12U and 18U 

Environment:
All versions and serial ranges.

Cause:
A customer is asking for details on the roof of the NetShelter SX 12U and 18U cabinets. 

Resolution: 
The roofs are not the same as the 42U and taller NetShelter SX cabinets. The roof is solid, and will not support troughs or ladder. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.