Browse FAQs

SNMPv3 changes not applied when done through CLI/Telnet

Published date: 14 February 2019

Issue
When applying changes to SNMPv3 settings through the CLI or telnet, changes are not actually applied until hitting "submit" in the web interface

Product Line
Network Management Card 1 (NMC1) - AP9617, AP9618, AP9619

  • Network Management Card 2 (NMC2) - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/AP9635CH 
    Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products.
     
Environment
 
  • All serial numbers
  • Any device listed above utilizing SNMPv3
 

Resolution
The current workaround is to apply intial changes and configuration using SNMPv3 through the web interface - or logging into the web interface after pushing changes and clicking the "submit" button. When a fix is available, this article will be updated with the proper firmware rev.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.