Browse FAQs

Is NetShelter SX shock packaging available for sale? Can an SX cabinet be converted into an SX Shock Packaging (SP) cabinet?

Published date: 18 January 2019

Issue:
A customer wishes to purchase part or all of the SP components. 

Product Line:
NetShelter SX Shock Packaging Cabinets

Environment:
All versions and serial ranges.

Cause:
A customer would like to convert an SX cabinet into an SX Shock Packaging cabinet. 

Resolution:

Pre-existing NetShelter SX cabinets cannot be converted in the field into SP cabinets. Adding the packaging and pallet does not convert an SX cabinet into an SP cabinet. 
The NetShelter SX SP (Shock Packaging) cabinets  are not the same as the stnadard SX cabinets.
Only NetShelter SX SP (Shock Packaigng) cabinets are tested and rated for shipping with eqiupment installed, to the rated load limit. 
The pallet and packaging for NetShelter SX Shock Packaging (SP) cabinets are not available as Spare Parts. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.