Browse FAQs

How to roll back NetBotz firmware.

Published date: 19 February 2019

Issue:
How to roll back NetBotz firmware.
 
Product Line:
Netbotz
 
Environment:
NetBotz 3xx, 4xx, and 5xx firmware
 
Cause:
If for some reason you feel the need to revert back to a previous firmware (BotzWare) revision on a NetBotz appliance, you can not simply use the upgrade feature.
 
 
Resolution:
Follow the detailed instructions for the TFTP procedure highlighted in FAQ FA176133.

Replace step 1 with the version of BotzWare to which you are looking to downgrade. Older revisions may be available at: www.apc.com/tools/download

Please note that when downgrading, it is suggested that you not keep any of the old configuration and do not use the "rootupgkeep" option in step 17.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.