Browse FAQs

NetBotz 250 | Managing Wireless Coordinator and Sensors

Published date: 20 December 2018

Issue:
Process for managing wireless coordinators and sensors on the NetBotz 250.

Product Line:
NetBotz 250 (NB250)
NetBotz Wireless

Environment:
NetBotz 250 (all versions)
NetBotz Wireless Sensors (NBWS100T & NBWS100H)
NetBotz Wireless Coordinator (NBWC100U)

Resolution:

Discovering Wireless Sensors - Auto Join
1) Log into the NetBotz 250 Web Interface.
2) Configuration Menu > Device > Wireless Sensor Network.
3) Click the Enable Auto Join button.
4) Turn on the wireless sensors.
NOTE: It is recommended to add one at a time and assigned a label to each one by clicking on the name of the wireless sensor.
5) When finished, disable auto join.
NOTE: If you forget to disable Auto Join it is will automatically disable after 5 hours.

Discovering Wireless Sensors - Manual
1) Log into the NetBotz 250 Web Interface.
2) Configuration Menu > Device > Wireless Sensor Network.
3) Click the Add New Sensor button.
4) Provide a wireless sensor name.
5) Enter the Extended Address which is located on the back of the sensor.
6) Enter a detailed location as to where the sensor is installed.
7) Edit the thresholds for the sensor.
8) Click Apply and ensure that the sensor shows within the Wireless Sensor Commission List.
NOTE: It may take a few minutes for the information within the Commission List to populate.

Editing Wireless Sensor Thresholds
1) Log into the NetBotz 250 Web Interface.
2) Configuration Menu > Device > Wireless Sensor Network.
3) Click on the name of the wireless sensor.
4) Edit the thresholds as necessary and click Apply.

Viewing Wireless Sensor Values
1) Log into the NetBotz 250 Web Interface.
2) Status Menu > Wireless Sensor Network.
3) Values are shown within the list for the sensors.
NOTE: If you have multiple sensors it is recommended to populate the Location field so you know exactly where each of them are installed.

Editing the Location Value of Wireless Sensors
1) Log into the NetBotz 250 Web Interface.
2) Status Menu > Wireless Sensor Network.
3) Click on the Wireless Sensor name.

Upgrade Wireless Sensor Firmware
Instructions for updated NetBotz Wireless Coordinators and Sensors can be found on the Help Center:
https://help.ecostruxureit.com/display/public/UANB250/NetBotz+Wireless+Sensor+Update+Utility+help+v1.0.1.03

Deleting Wireless Sensors
1) Log into the NetBotz 250 Web Interface.
2) Configuration Menu > Device > Wireless Sensor Network.
3) Click on the wireless sensor name that you wish to remove.
4) Click on the name of the wireless sensor again.
5) Click the Remove button at the bottom.

Fully disabling all wireless capabilities on the NetBotz 250
Remove the coordinator from the appliance.  The coordiantor is located under a plastic cover on the front of the appliance.  If you are unsure of the exact location of the coordinator, see the diagram within the installation and quick configuration guide:
https://help.ecostruxureit.com/display/SWDCDOC/PDF+Library?preview=/96044657/132647262/990-9814C.pdf#PDFLibrary-CompleteGuide.3

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.