Browse FAQs

What is the total length requirements for the Hilti anchors used in IBC and OSHPD seismic anchoring?

Published date: 11 December 2018

Issue:
A customer wants to know the total anchor height. 

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
The IBC and OSHPD seismic documents only show hole depth. Customers need to know the how much anchor is needed above the floor too. 

Resolution:


Attached is a link to the technical information for the Hilti Kwik bolts that are specified to be used. Based on the length of the anchor used and the depth of the hole drilled, you can determine the height from the floor to the top of the fastener from the chart provided on the Hilti Kwik spec sheet: https://www.hilti.com/medias/sys_master/documents/hac/9233455513630/Technical-information-ASSET-DOC-LOC-1543424.pdf
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.