Browse FAQs

Short Circuit Rating of SYBTU1-PLP & SYBTU2-PLP Batteries

Published date: 03 August 2018

Issue:
Request for the short circuit ratings of the SYBTU1, and SYBTU2 batteries.
 

Product line:
Symmetra PX, Smart UPS VT
 

Environment:
All models, all serial numbers
 

Cause:
Request for information on the short circuit ratings of the battery modules used in the Symmetra PX and Smart UPS VT systems.
 

Resolution:
The short circuit rating of the battery module is limited by the fuses inside it.  The SYBTU1-PLP, and SYBTU2-PLP battery modules have fuse part #515-1063-Z.
Fuse Fast 63 Amp 500 VDC / 690 VAC ROHS
 
Bussmann Spec Sheet attached.
 

 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.