Browse FAQs

Can AR7580A be installed into the 45U NetShelter SX?

Published date: 19 July 2018

 Issue: 
We need to determine if the 42U finger-style vertical cable managers will fit into a 45U NetShelter SX cabinet. 

Product Line: 
NetShelter SX, NetShelter Vertical Cable Management

Environment: 
AR7580A, AR3155, AR3355 all serial numbers. 

Cause: 
Availability issues with AR7585 may create the need to use 42U cable managers. 

Resolution: 

AR7580A will install into the 45U NetShelter SX cabinet but there will be no cable management fingers U-spaces 1 thru 4.  
Mounting it in this manner will allow the thru-holes of the mounting rails and cable managers to align. 
Please see the attached document. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.