Browse FAQs

Can the AR8395 busbar install into a NetShelter SV? The busbar installs at three points, but the cabinet only has two accessory mounting brackets.

Published date: 16 July 2018

Issue: 
The AR8395 busbar has three installation points. 

Product Line: 
NetShelter SV, AR8395

Environment: 
All models, all serial numbers. 

Cause: 
NetShelter SV cabinets ship with two accessory mounting brackets. 

Resolution: 
The AR8395 busbar is compatible with NetShelter SV cabinets, but it does require an extra accessory bracket (AR824002).
See attached file.  

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.