Browse FAQs

The “Generic Modbus” application does not provide status bits values in binary

Published date: 12 July 2018

Issue:
The “Generic Modbus” application does not provide status bits values in binary


Product line:
Generic Modbus Application or Similar application


Environment:
Generic Modbus Application or Similar application


Cause:
The “Generic Modbus” application does not provide status bits values in binary


Resolution:
Take the value provided by the application and convert it to binary by using a calculate like the one provided by Windows.  If using the Windows calculator, you may have to change the calculator to scientific or Programmer mode to accomplish this conversion.
Below is a couple of examples from a Galaxy VX:
Example 1:  Register 400002 (16385)
16385 in BIN 100 000 0000 0001
This example has 14 bits and to get to 16 bits two zeros were added to the left (red text)
10 0000 0000 0001 is 0010 0000 0000 0001
 
Example 2:  Register 400010 (512)
512 in BIN 10 0000 0000
This example has 10 bits so six bits needs to be added to the left (red text)
10 0000 0000 is 000 0010 0000 0000

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.