Browse FAQs

Do the 800 mm wide NetShelter SV cabinets have 1U rackmount spaces in the vertical mounting rails?

Published date: 26 March 2019

Issue: 
This space would be perfect to mount small IT devices into. 

Product Line: 
NetShelter SV 

Environment: 
800 mm width only, all serial numbers. 

Cause: 
It appears there may be a 1U punch out in the vertical mounting rails. 

Resolution: 

Yes, all of the NetShelter SV 800 mm wide cabinets have EIA 1U punch outs with square mounting holes. These spaces can be used to mount small IT devices, cable management, PDU...etc. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.