Browse FAQs

Is the PDU removable that's included inside the NetShelter CX AR4000MV?

Published date: 13 March 2019

Issue: 
A customer wants to replace the PDU in a NetShelter CX Mini. 

Product Line: 
NetShelter CX

Environment: 
AR4000MV, all serial numbers. 

Cause: 
The brochure doesn't show if the PDU is removable. 

Resolution: 

The PDU that ships installed inside the AR4000MV is removable. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.