Browse FAQs

What size bolts are needed to floor mount the NetShelter 4-post rack?

Published date: 13 March 2019

Issue: 
A customer needs to know what size bolt will fit through the floor mounting holes in the rack. 

Product Line: 
NetShelter SX

Environment: 
AR203A, AR204A, all serial numbers. 

Cause: 
There is no documentation as to the size of the floor mount holes. 

Resolution: 

A 5/8" diameter bolt (19 mm) will fit through the floor mount holes of the NetShelter 4-post rack. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.