Browse FAQs

NetBotz appliance configuration resets to default with Rack Access pod connected.

Published date: 10 June 2019

Issue:

NetBotz appliance config gets wiped out after a period of time with Rack Access 170s connected.

Product Line:

NetBotz

Environment:

NBPD0170, NBPD0170, NBPD0172
Supported NetBotz appliance

Cause:

On Botzware prior to 4.5.2, If a NetBotz Rack Access pod 170 label is changed, subsequent HID card swipes will cause increasing corruption on the NetBotz appliance. Eventually this will cause an issue where the device will lose it's configuration.

Resolution:

If you are running into this issue, you will need to reset the appliance to default then upgrade to 4.5.2 or higher. If you do not reset the configuration or if you pull a backup from prior version that had the issue, the issue will potentially continue to happen. K-base FA158175 explains how to reset the NetBotz configuration or do a "configreset" on a NetBotz appliance.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.