Browse FAQs

Video: How to calibrate fuel levels on an ISX-ATS-GEN

Published date: 08 May 2018

Issue:
Calibrating Generator Fuel Level to 100% on SmartGen ATS with ISX
 
Product line:
APC ISX-ATS-GEN
 
Environment:
All Product models, all serial numbers
 
Cause:
The ATS needs to have the generator fuel level reset any time the generator tanks are full.

Resolution:
Go through the steps for calibrating the fuel level on an APC ATS. This procedure should be completed when the generator is 100% full.

Select ‘Config’ from the Main menu
Select ‘Calibrate Fuel Level’
Select ‘Yes” to confirm

The display will show (***Cal Fuel Level to xxxxx) 

The following video demonstrates this procedure:
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.