Browse FAQs

What are the factors that affect Battery Rated Service Life?

Published date: 28 January 2018

Issue:
What are the factors that affect Battery Rated Service Life?
On paper, batteries are given a design life of 5 years, 8 years, 10 years, etc.  They get weak, or fail sooner than there rated lifespan.  That is their Service Life
 
Product line:
Symmetra, Galaxy, EPS, Smart UPS, Battery
 
Environment:
All models, all serial numbers
 
Cause:
The design life is the life expectancy the manufacturer says the battery is capable of, provided that all of the specification parameters are maintained.
 
The main things that affect battery service life.
1)Design Life -
Float voltage accuracy
Frequency of discharges
Number of discharges
Maximum discharge rate
Depth of discharges
End voltage limit
Operating temperature
The amount of ripple current and voltage allowed, during charging as well as discharging. This is a very strict regimen that has to be followed very accurately in order to achieve the Design Life. Not many installations can maintain that level of control.
 
2)Temperature – The standard is 25 C (77 F).  
•  This specification is for the internal temperature of the battery, and not for the ambient room temperature. 
Keep in mind if batteries are installed inside a cabinet, the internal temperature of the battery is usually 2 deg warmer than ambient air, and temperature at the top of the cabinet can be 10 F warmer, than at the bottom.
CAUTION: Battery life is halved for every 10°C above 25°C.
 
3)Duty Cycle – This is how often the battery charges and discharges.
 
4)Environment -   The VRLA battery is specifically designed to be installed
in occupied spaces, meaning the places where people normally work. 
Corrosive environments are not places where people normally work.  Care must be taken to ensure that the environment is not corrosive.
Charge / Float Voltage
Charge Maximum Current
AC Ripple
Maintenance of fluid levels, terminal torques.
 
Resolution:
If one looks at these terms, and considers them with the simplest explanation, it is easy to see that Design Life is the life expectancy the manufacturer says the battery is capable of, provided that all of the specification parameters are maintained. It is also relatively easy to see that, because of the real-world physical and electrical environmental variables, it is highly unlikely that the Service Life will be anywhere near the Design Life.
 
Reference:
Sample Battery Spec Sheet: CSB-HRL-1234W-F2FR.  Page two has various charts to estimate the effects of duty cycle, battery storage, and temperature on service life.  These types of spec sheets can be obtained from the battery manufacturer.
 
APC_WHITE_PAPER 230: Lead Acid Battery Lifecycle
 
 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.