Browse FAQs

​PowerChute Business Edition - Supported UPS Models

Published date: 12 August 2020

Issue:
There are two new categories to consider when manually selecting a UPS during PowerChute Business Edition installation.

Product Line:
PowerChute Business Edition version 9.5 and higher

Environment:
All supported operating systems when connected to a Smart-UPS


NOTE: Back-UPS are not compatible with PowerChute Business Edition. Back-UPS are compatible with PowerChute Personal Edition when connected to a computer running Windows OS 7, 8, 10

Cause:
Updates to the PowerChute Business Edition v9.5+ installation process.

Resolution:

During installation of PowerChute Business Edition v9.2.1 and earlier, PowerChute asks you to check the monitoring ports on the back of the UPS (DB9 or RJ45) to determine the type of UPS that you want to manage.
From PowerChute Business Edition v9.5+, you are instead asked to select your UPS from a list of UPS model prefixes (e.g. SMT, SMX, SMC, SU etc.).
Your UPS model is printed on the label at the back of your UPS.
All supported UPS models are categorized into two types:
  • Type-A Smart-UPS models with prefix SMT, SMX, SURTD, SRT, SMTL
    (including models SRC2KUXI, SRC3KUXI, and SRC3KUXIX709)
  • Type-B Smart-UPS excluding UPS models with prefix SMT, SMX, SURTD, SRT, SMTL
If you are not sure to which category your UPS belongs, check the table below for the latest models:
Type-A UPS Type-B UPS
SMT SU
SMX SUA (including C500J)
SMC SURT
SURTD SURTA
SRT SC
SMTL SUM
SCL  
   
SRC models:
  • SRC2KUXI
  • SRC3KUXI
  • SRC3KUXIX709
     
Any SRC model, excluding those listed under Type-A.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.