Browse FAQs

Why does uninstall script for PowerChute Network Shutdown 4.2 not properly clean up firewalld on RHEL 7.3 and CentOS 7.3?

Published date: 07 May 2019

Issue:
uninstall script for PowerChute Network Shutdown 4.2 does not properly clean up firewalld on RHEL 7.3 and CentOS 7.3

Product:
PowerChute Network Shutdown version 4.2

Environment:
RHEL 7.3 and CentOS 7.3

Cause:
From RHEL 7.3 release notes, firewalld packages have been upgraded to provide some enhancements over its previous version. Which includes changes in the firewall-cmd, firewall-offline-cmd, firewall-config, and firewall-applet.

Solution:
After running the PowerChute uninstall script run the command 

firewall-cmd --remove-service=pcns --permanent

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.