Browse FAQs

Where do I find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC modular batteries

Published date: 25 January 2018

Issue:
Where to find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC modular batteries
 

Product line:
SYBTU1-PLP / SYBTU2-PLP
 

Environment:
PX1,2, 250-500, SUVT and Galaxy 3500
 
 
Information:
See application note 143 for specific values of contained electrolyte in both the SYBTU1-PLP (used in PX1 20,40, 48, 80 and 96KVA UPS units as well as the SUVT and Galaxy 3500 UPS units) and the SYBTU2-PLP (used in the PX2 100KVA and the PX 250/500KVA UPS units) batteries.
Application Note 143:
https://www.apc.com/salestools/SMCR-6NXGXU/SMCR-6NXGXU_R2_EN.pdf
 
 
Note – SYBTU1-PLP and SYBTU2-PLP use batteries manufactured by four different vendors. For further information on MSDS by the specific vendors please refer to FA157067
 
 Also see FA FA157067
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.