Browse FAQs

Are there instructions showing the proper way to install the gasket material of a Vertical Exhaust Duct Kit?

Published date: 02 May 2019

Issue:
Pieces of the gaskets are loose or falling off.  

Product Line: 
Vertical Exhaust Duct Kits

Environment: 
All versions and serial ranges 

Cause: 
If the gasket is not installed properly it will not adhere. 

Resolution:
See attached file.  

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.