Browse FAQs

PowerChute Network Shutdown will not communicate with or drops communication with VMware ESXi 5.5 host

Published date: 21 February 2019

Issue:
PowerChute Network Shutdown will not communicate with or drops communication with VMware ESXi 5.5 host.
In the PowerChute error.log file the error Connection to ESXi Host could not be made.java.rmi.RemoteException: VI SDK invoke exception:javax.net.ssl.SSLHandshakeException: Remote host closed connection during handshake is recorded. 

Product Line:
PowerChute Network Shutdown versions 4.X

Environment:
Vmware ESXi 5.5 host

Cause:
VMware service patch

Solution:
Install the latest VMware patch ESXi550-201612001
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.