Browse FAQs

How quiet (or noisy) is the NetShelter CX when only the fans are running, with no equipment installed?

Published date: 24 January 2019

Issue:
Customer wants to know how quiet the cabinet is with nothing installed, just the fans running. 

Product Line:
NetShelter CX

Environment: 
All versions and serial ranges.

Cause:
Noise reduction in the office is important. 

Resolution: 

Noise of AR4018A / AR4018IA:
40.5 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet
 
Noise of AR4024A / AR4024IA:
43.0 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet
 
Noise of AR4038A / AR4838IA:
43.5 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.