Browse FAQs

Video: How to change the Maintenance Intervals on a Network Air FM unit

Published date: 25 September 2018

Issue:
How to change the Maintenance Intervals on a Network Air FM unit.
 
Product line:
FM35-50, ACFM, IR40.
 
Environment:
All Serial Numbers.
 
Cause:
Install Operation.
 
Resolution:

 
How to change the Maintenance Intervals on a Network Air FM unit follow the below procedures.
 
1 Press ESC until you reach the main menu (On/Off).
 
2 Scroll to SETUP and press ENTER.
 
3 Scroll to SYSTEM 1 and press ENTER.
 
4 Press ENTER on ALARMS.
 
5 Press ENTER on MAINT ALARMS.
 
6 Press ENTER to scroll through the device available.
1 of 7 Compressors 1
2of 7 Compressor 2
3 of 7 Heaters
4 of 7 Blowers 1
5 of 7 Blowers 2
6 of 7 VFD 1
7 of 7 VFD 2
 
7 Press ENTER on the selected device.
 
8 Press the DOWN arrow once then press ENTER again.
 
9 Using the UP or DOWN arrows you can select the desired interval or disable this feature.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.