Browse FAQs

What are the hole sizes and dimensions of the AR8395 copper bus bar?

Published date: 05 August 2019

Issue:
A customer wants to use 2-hole lugs on the ground bar

Product Line:
NetShelter Bus Bar

Environment: 
AR8395

Cause:
Grounding / bonding is required

Resolution: 
The AR8395 has the following holes available: 
47 holes threaded #10-32, spaced 18 cm center to center. 
25 holes at 5.5 cm and 9 holes at 7.9 cm, spaced at 25 cm center to center. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.