Browse FAQs

NetBotz 250 has delay showing A-Link sensors in web interface during initial discovery.

Published date: 11 May 2018

Issue:

NetBotz 250 has delay showing A-Link sensors in web interface during initial discovery.

Product Line:

NetBotz

Environment:

NetBotz 250

Cause:

When you initially connect an AP9520T or AP9520TH A-link sensor to a NetBotz 250, the device may not show the sensor for 3 to 4 minutes.

Resolution:

This issue should only occur when the A-link sensors are initially connected. When simply launching to the web page of the device after the sensor is discovered should show up as soon as you open the page to view that sensor.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.