Browse FAQs

If a NetShelter CX is scratched or dented can it be repaired? What color is the finish?

Published date: 18 June 2019

Issue:
A customer may want to touch up or repair damage to a NetShelter CX cabinet. 

Product Line:
NetShelter CX

Environment: 
All versions and serial ranges.

Cause: 
A NetShelter CX cabinet has been scratched or damaged. 

Resolution:
There are a couple of options a customer can use to disguise damage, but at closer inspection any repair work will remain visible. In most cases the repair will be visible. 
A color marker can help cover a scratch. To fill a hole or indentation it may be necessary to first fill it, then paint it. 
These are the colors that will patch: 
RAL - 7016
NCS - S8000-N
Pantone - 433U

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.