Browse FAQs

Video: How to configure Modbus on an InRow ACRD200 cooling system

Published date: 27 April 2018

Issue:
How to configure Modbus on an ACRD200 cooling unit

Product line:
InRow RD

Environment:
All Serial Numbers

Cause:
Install, Configuration

Resolution:



Press ESC until you get to the main screen (On/Standby)
 
Use the Up or Down arrows to find the heading Configure Modbus
 
Press ENTER and select Modbus
 
Now you will be prompted for a password
 
Use the default password of “apc”
 
If this does not work check with your Admin for the correct password
 
If password has been lost use the last eight digits of the serial number
 
Press Enter again on Modbus and you can select either Enable or Disable
 
Select ID and you can select an ID number for this unit between 1 and 247
 
Select Baud Rate and you can choose either 9600 or 19200.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.