Browse FAQs

ACF400 Spare parts break down

Published date: 25 January 2018

Issue:
ACF400 Spare parts break down

Product line:
ACF400, ACF115, ACF136

Environment:   
Air Removal Unit
 
Cause:    
  
Resolution:     
Please call tech support at 1-888-695-6500 and hit option to three times to get to the cooling team to verify part numbers before ordering, as they may change.

ACF400 break down
This is the entire fan and power system.
ACF115          APC Rack Air Removal Unit SX Fan Assembly 100-240V 50/60 Hz (All 4 fans and Electronics module included)
ACF136          APC Rack Air Removal Unit SX 600mm Wide Frame
ACF126          Ducting Kit
W0M-7053     ASSY ARU GEN 2 ELECTRONICS MOD
W0M-7054     AIR REMOVAL UNIT G2 REPLACEMENT FAN MODULE
0J-0G-9233     GENERIC ANSI WWPV LCD DISPLAY
0J-0W2818A  Temperature Sensor (Optional)
AP9324           Beacon (Optional)
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.