Browse FAQs

Video: How to clean a Condensate drain line on an ACSC100 unit

Published date: 29 May 2019

Issue:
How to clean a Condensate drain on a ACSC100 unit..
 
Product line:  
ACSC100 and ACSC101
 
Environment:  
All Serial Numbers...
 
Cause:  
Clog due to debris or sediment
 
Resolution:  
See Attached video
 
This video will show you how to remove and clean clogged drain lines and clogged condensate pumps on an ACSC100 unit.  Ensue the unit is powered off then unplug the unit from power.  When using compressed air please ensure safety glasses are used.  Will also need to create a seal to slightly pressurize the line.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.