Browse FAQs

Are the new 6U, 9U and 12U NetShelter cabinets hinged in the rear, like AR100 & AR100HD?

Published date: 02 May 2019

Issue:
Customers inquire if the newer 6U, 9U and 12U wall mount cabinets are hinged in the rear.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
The 13U NetShelter WX cabinets are hinged in the rear.

Resolution:
The new 6U, 9U and 12U NetShelter WX cabinets (AR106, AR109, AR112) are not hinged in the rear. Only the NetShelter WX AR100 and AR100HD are hinged in the rear,

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.