Browse FAQs

Which parts of a NetShelter cabinet are considered user replaceable?

Published date: 12 March 2019

Issue:
Need to determine which NetShelter components can be replaced by customers in the field.

Product Line:
NetShelter SX, SV, VX

Environment:
All versions and serial ranges.

Cause:
A part of the cabinet has been damaged and needs to be replaced.

Resolution:

Many parts of the cabinet are designed to be user replaceable: roof, side panels and doors.
The user manuals show how to replace these parts. The manuals are available on the APC website.
  • The roof can be removed by disengaging two hinge pins, then they simply lift off. NOTE: The NetShelter SV roof is not removable. 
  • The sides can be removed by unlocking them, then they simply lift off.
  • The doors can be removed by disconnecting the ground wire, then they simply lift off.
If cabinet parts are damaged in transit by a Schneider Electric carrier (Shipped from Schneider Electric, Freight Prepaid & Add) we will send user replaceable parts-only free of charge. Installation is not included. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.