Browse FAQs

Can the Combination Lock Handle or PX-HID Lock be installed onto the ARU?

Published date: 11 March 2019

Issue:
Customer requests compatibility information between the Combination door handle or PX-HID lock, and the ARU.

Product Line:
NetShelter SX ARU, NetBotz PX-HID

Environment:
All versions and serial ranges.

Cause:
Customer requires secure access to the ARU.

Resolution:
The Combination Lock Handle and PX-HID Lock are not compatible with the ARU. 
If additional security is required, the lock cylinder can be replaced to accept a unique key, as described in FAQ FA158606: https://www.apc.com/us/en/faqs/FA158606/ 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.