Browse FAQs

How much space is available in the NetShelter WX AR100 from the front rail to the door?

Published date: 28 August 2018

Issue:
Customers may need to know how much space is available between the front mounting rails and the front door.

Product Line:
NetShelter WX

Environment:
AR100 and AR100HD, all serial ranges.

Cause:
Customers may need to use the space between the mounting rails and front door in the NetShelter WX.

Resolution:
With the front mounting rails in their forward position as shipped from the factory there's approx. 3" of space available from the mounting rails to the front door.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.