Browse FAQs

Do the Cisco Nexus 7700 series switches require a side airflow duct kit?

Published date: 24 June 2019

Issue:
Customers ask if the Nexus 7700 series also requires side airflow duct kits.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
The Cisco Nexus 7000 series switches utilize side airflow and required large volumes of air to cool properly. Duct kits are used to help the switches cool efficiently and prevent hot air recirculation.

Resolution:

The Cisco Nexus 7700 series switches use front-to-rear airflow and do not require side airflow duct kits.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.