Browse FAQs

Which Smart Slot Accessories are compatible with the SRT series of Smart-UPS Online products?

Published date: 10 September 2018

Issue:
Which Smart Slot Accessories are compatible with the SRT series of Smart-UPS Online products?
 
Product Line: 
 
Smart-UPS Online
 
Environment: 
 
All SRT models, All Serial Numbers 
 
Cause: 
 
The SRT series is an all new generation of Double Conversion Online Smart-UPS. The updated UPS platform does not support all legacy accessory cards.
 
Resolution:
 
The following accessory cards are currently compatible with all SRT models:
AP9630, AP9631 Network Management Cards - Requires firmware SUMX v618 or later
AP9613 - Dry Contact Relay I/O Card
AP9620 Legacy Communications Card
 
In addition, SRT models 5Kva and larger include an embedded Network Management Card.
The embedded NMC supports the following accesories: 
AP9335T (temperature probe, supplied with UPS)
AP9335TH (temperature and humidity probe) 
AP9810 (relay I/O dongle) through the universal I/O port on the back of the UPS

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.