Browse FAQs

Can a cooling unit be tipped or moved on its side?

Published date: 02 May 2019

Issue:
Can a cooling unit be tipped or moved on its side?

Product line:
All Units 

Environment:
Data Center Cooling

Cause:

Resolution:

The Inrow units are not designed to be tipped off center or placed on their sides for movement. The units have a high center of gravity and tipping is a safety concern as documented in the O&M manual.  Parts cannot be removed from the unit.  THIS WILL VOID ALL WARRANTY. Please see below for the maximum amount of degrees that is allowed to be tipped.  Caution must be taken when moving these units.

ACSC10x       0
ACRC10x       0
ACRC30x       0
ACRC50x       0
ACRD10x       0
ACRD20x       0
ACRD50x       0
ACRP10x       0
ACRP50x       0
Uniflair            Less than 10 Degrees 
Stulz              Less than 10 Degrees
FM                 Less than 10 Degrees
Airflow            Less than 10 Degrees


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.