Browse FAQs

Does the NetShelter CX interfere with a device's wifi signal? If it does, by what degree is the signal strength reduced?

Published date: 26 March 2019

Issue:
Need to determine if the NetShelter CX can effect wifi signal strength.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Wireless devices can be installed inside a NetShelter CX cabinet.

Resolution:
A wireless device was tested in the NetShelter CX manufacturing facility. The signal strength was affected by less than 10% in 3 of the test areas and by 38.46% in 1 of the areas. The test results show that the Office had the greatest signal reduction but only dropped to a Fair signal strength. None of the results indicated a poor or unusable signal.

A complete test report is attached below.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.