Browse FAQs

In Hyper-V, Virtual Machine shutdown is delayed when VM Migration is enabled.

Published date: 06 December 2018

Issue:
There is a delay proceeding with virtual machine shutdown when VM migration is enabled for Hyper-V.

Product Line:
PowerChute Network Shutdown v3.1 and above

Environment:
Windows Hyper-V

Cause:
If the VM Migration time is insufficient in attempting to migrate all VMs, there is a timeout issue before PowerChute proceeds with shutting down VMs that failed to migrate.

Resolution:
Ensure you allow sufficient time for the the VM migration duration to attempt to migrate all VMs.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.