Browse FAQs

What is capacity regulation on an ACRD?

Published date: 15 January 2018

Issue:
What is capacity regulation on an ACRD?

Product line:
ACRD100, ACRD101, ACRD200, ACRD201

Environment:
Data Center Cooling

Cause:

Resolution:
Capacity regulation is a method of controlling the capacity of the InRow ACRD unit. This is achieved using an electronic Hot Gas Bypass Valve (HGBV) which allows the unit to operate at low load conditions down to 2.5 KW without compressor recycling.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.