Browse FAQs

What is the input voltage required for the InRow ACRD?

Published date: 15 January 2018

Issue:
What is the input voltage required for the InRow ACRD? 
 
Product line:
ACRD100, ACRD101, ACRD200, ACRD201
 
Environment:
InRow Cooling
 
Cause:
 
Resolution:
The InRow ACRD unit uses a single phase 208V/60Hz input in NAM and a 230V/50Hz input in the rest of the world.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.