Browse FAQs

Can the condensate pump for the 600mm units provide more lift if the capacity is de-rated?

Published date: 11 April 2019

Issue:
Can the condensate pump for the 600mm units provide more lift if the capacity is de-rated?

Product line:
ACRP1XX, ACRP5XX, ACRD5XX, ACRD5XX.

Environment:  
All Serial Numbers.

Cause:  
Install, Repair.

Resolution:
The pump does have some degree of lift compensation as many other pumps do. As the head decreases, the pump volume is reduced. The maximum shutoff is 19ft of head. The data for flow versus lift follows:
 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.