Technical FAQs

Ask a Question

Are there any user replaceable parts in the ACSC1XX ?

Issue:  
Are there any user replaceable parts in the ACSC1XX ?

Product line:
ACSC1XX.

Environment:  
All Serial Numbers.

Cause:
Install, Repair.

Resolution:

Yes, the filter at the rear of the unit is washable and replaceable. Also, the evaporator fans and fan power supplies are hot
swappable through the front of the unit.
 
How to install or remove a Evaporator Fan from a ACSC100 or ACSC101 unit.
 
How to change fan power supplies in an acsc unit
Was this helpful?
What can we do to improve the information ?