Browse FAQs

Can I run cables over the SC? If so, how many?

Published date: 11 April 2019


Issue:  
Can I run cables over the SC? If so, how many?

Product line:
ACSC1XX.

Environment:  
All Serial Numbers.

Cause:  
FAQ.

Resolution:
 
Yes, there is a cable support bridge trough available as an accessory (ACAC10021). You will need (2) per SC unit to carry
both data and power cables across the unit. Approximately 80 CAT5 cables or 8 power whips fit into a trough.
 
 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.