Browse FAQs

What should I do if all or some of the fans in a NetShelter CX fail or are noisy?

Published date: 12 November 2018

Issue:
NetShelter CX fan is noisy or has failed.

Product Line:
NetShelter CX
 
Environment:
All versions and serial ranges.
 
Cause:
There are several possible causes for fans to be noisy or fail.
 
Resolution:
 

All fans in the fan tray stop.

Possible cause - Power supply has failed: broken wire or loose connection.
Field solution - Check that the power supply unit LED is illuminated.
                       Check all power connections to power supply and fan tray and if necessary, change the power supply.

Single fan failure

Possible cause - Damaged fan frame, failed bearing etc.
Field Solution - Replace fan tray.

Noisy Fan  

Bearing noise or ticking blades.
Possible cause - Distorted or broken fan frames, bearing lubricant failed due to age or excessive temperatures or something catching the blades such as tape. etc.
Field solution - Check for anything interfering with free rotation of the blades. Check to make sure fan is seated correctly in the fan tray. If nothing is obvious, change the fan tray.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.